cancel
Showing results for 
Search instead for 
Did you mean: 

IOC File Not Displaying Diagram

RHJ
Associate II

I upgraded STM32Cube IDE to 1.12.0, and now when I double-click the IOC file, it just displays a text file, not the processor pin / configuration diagrams, etc.  I tried closing and re-opening the project(s) and closing and re-opening CubeIDE.  No change.

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Probably your workspace was created in 1.12.0. It's just a directory name now, not the product version.

Yes you can downgrade if you want.

STM32CubeIDE | Software - STMicroelectronics

TDK_0-1764772678440.png

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

5 REPLIES 5
TDK
Super User

STM32CubeIDE v2.0.0 does not support IOC files natively.

Use standalone STM32CubeMX to view and generate code.

STM32CubeIDE 2.0.0 released - STMicroelectronics Community

If you feel a post has answered your question, please click "Accept as Solution".
Karl Yamashita
Principal

1.12.0 is like over 2 1/2 years old. At least upgrade to 1.19.0

Starting with STM32CubeIDE 2.0.0, you'll need to use STM32CubeMX to create the IOC.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

RHJ
Associate II

I'm a little confused about the version number.  The About page says 2.0.0 but the top of the workspace says 1.12.0.
Anyway, I'd prefer to have the config tool incorporated in the IDE.  Can I downgrade to 1.19.0?

TDK
Super User

Probably your workspace was created in 1.12.0. It's just a directory name now, not the product version.

Yes you can downgrade if you want.

STM32CubeIDE | Software - STMicroelectronics

TDK_0-1764772678440.png

 

If you feel a post has answered your question, please click "Accept as Solution".
RHJ
Associate II

Not really what I'd prefer, but I guess that's the answer.