STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1556 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 590 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

HardFault_Handler

Hello,until recently, I used the STM32F411CEU6 microcontroller; lately, I switched to the STM32G0B1.I've ported the old C++ code from the STM32F411CEU6 to the STM32G0B1.Everything works correctly; the only issue is that now, 'HardFault_Handler()' occ...

Resolved! In STM32CubeIDE How can I fix "arm-none-eabi-gcc: fatal error: cannot execute 'cc1': CreateProcess: No such file or directory"

When I create the default project for the NUCLEO-F429ZI board and build without any edits I get the following error repeatedly and would like to get rid of it. I can build the same on a different laptop. How can I solve this problem. "arm-none-eab...

jdsotack by Associate II
  • 10963 Views
  • 3 replies
  • 2 kudos

ADC

how to use multiple adc in stm32f746zg nucleo board

STM32CubeIDE 1.14 and Darkest Dark Theme with DevStyle

I uninstall IDE v1.13 and install the new v1.4 from the ST website.Installation without problems, but already at the first launch I see that instead of the Information Center page it says "the page cannot be displayed".When I try to download Darkest ...

KHans.4 by Associate
  • 3257 Views
  • 1 replies
  • 0 kudos

Resolved! ThreadX priority

Hi guys. Help solve this problem.I am working with STM32H745 and ThreadX. In my project, an external event generates an interrupt on EXTI10.The tx_event_flags_set() function is executed from the HAL_GPIO_EXTI_Callback() interrupt handler to start a p...

Resolved! STM32g0xx change boot address with option bytes

Hi, I used this code to change the boot address in the STM32U575 project:FLASH_OBProgramInitTypeDef OB_Data;/* Unlock Flash Control register and Option Bytes */HAL_FLASH_Unlock();HAL_FLASH_OB_Unlock();OB_Data.OptionType = OPTIONBYTE_USER | OPTIONBYTE...

MishKa59 by Associate II
  • 2083 Views
  • 2 replies
  • 0 kudos

unable to debug stm32f508-dk

sir i am trying to read and write 10 bytes of data into flash memory, before that iam going to debug the code ,am getting this error "No source available for "_binary_______ExtMem_Boot_Binary_Bootloader_bin_start() at 0x8001ece" "

kishor by Associate II
  • 2106 Views
  • 3 replies
  • 0 kudos

Multiple errors reported.

Hi, currently I have an issue during debug. I'm writing a bare metal code to blink a LED, when I compile the code there aren't any error occur. But when check the Expression I got this errors, I have search everywhere but I can't find the solution ye...

trietmt9_0-1702304937876.png
trietmt9 by Associate II
  • 3774 Views
  • 5 replies
  • 1 kudos