STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32cubeIDE SWV trace autostop

Hello,I am new on STM32CubeIDE. I try to use SWV to trace some parameters from Nucleo-H743ZI2. At the beginning, everything is ok. I can see the data in the trace window. But the trace will automatically stop after a certain duration. The board is st...

Capture.PNG
Jiaming by Associate III
  • 3653 Views
  • 4 replies
  • 1 kudos

Build issue - error directive usage

Hi All, I am having a strange error. When I compile my code, the error directive causes the ERROR. I can not pinpoint the issue. Could you please hint me in the right direction?Thanks and Regards,  

demir_0-1706300477525.png
demir by Senior II
  • 1636 Views
  • 2 replies
  • 2 kudos

Resolved! Conversion of int to float and float to int

Hello guys, I hope you're doing well, I'm currently trying to replicate a video I saw on YouTube about audio processing using stm, I'm just starting to develop for stm and I'm having some doubts, mainly in terms of libs. I'm trying to convert between...

STM32L072 LIN Communication

Hello everyone,I currently facing an issue. I can successfully send the break and sync byte, but for some reason, my ID is not being transmitted. When I switch from RDR to TDR in LIN_UART_ISRHandler, I can receive all the data from slave on the Picos...

Ofaro.1 by Associate II
  • 1443 Views
  • 0 replies
  • 0 kudos

Accuracy of internal RC oscillator of STM32F030C8

Hi ST Community,I am planning to design a board with STM32F030C8 that will be mass produces. It will be very small PCB, so I am plannig to use internal RC oscillator of the MCU. The MCU will use I2C1  (to write some data to LCD with I2C converter) an...

shydv15 by Associate II
  • 1871 Views
  • 1 replies
  • 2 kudos

Resolved! Include files help.

I have a source folder named components where each subfolder has a .c and a .h file, see screenshot below.I am trying to include these files, but they cannot be found. So far, I know that I should add the relative path and so I did. (I also tried to ...

ubaldot_0-1706174213811.png
ubaldot by Senior
  • 2764 Views
  • 2 replies
  • 1 kudos