STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1268 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 512 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! RE: How to change the Repository directory (location)?

A while ago I auto updated to 2.0.0. Prior to that, I was able to change the repository location. The instructions were nicely noted here: https://community.st.com/t5/stm32cubeide-mcus/how-to-change-the-repository-directory-location/m-p/114938 Now wi...

CCoder_0-1769098998082.png
C-Coder by Associate III
  • 358 Views
  • 2 replies
  • 1 kudos

Resolved! Share source files between multiple projects

Hi,at this moment I have two projects (BootLoader and Application), but I have some shared files.What is the best solution to share those files? Is it possible to create an 'empty' project, with only those shared files, and make the two projects depe...

ErX by Associate III
  • 402 Views
  • 3 replies
  • 1 kudos

Resolved! Cannot select multiple lines of text on macOS Tahoe 26.1

Eclipse and hence CubeIDE has this problem described here (and in the title):https://github.com/eclipse-platform/eclipse.platform/issues/2244#issuecomment-3533012572For Eclipse there is a patched version out there.Is there a timetable to get this fix...

nyholku by Associate
  • 437 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeIDE 1.19.0 does not show myST login

Hello all,I'm facing a wired issue. After the IDE update in the Help menu there is no more the entry to log-in in myST.Do you have any suggestion how to reach the myST login from it?I'm running the IDE on Windows. Thanks in advance!

Resolved! STM32CubeIDE 1.19.0: GCC generates wrong code

I have a simple function with loop that checks RX pin state for 10ms, and if there was high level - breaks loop and exits. it works ok with -O0, but is broken with -Os or -O1 (-O2) or -Og - it loops forever.Here's code:uint8_t isModemOn() { uint32_...

NiTr0man by Associate III
  • 240 Views
  • 2 replies
  • 1 kudos