STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

ST32F469I AU1 Serial port issue on Cube IDE

Hi All I am having difficulty getting the serial to work through the STlink on the STM32F469I AU1 (MB1189B) version. I have tried all the suggestions in the previous posts on the forms. The uart is set with the correct pins according to the schematic...

STMCube IDE problems with Queues

Im creating an RTOS queue in the configuration tool. Whowever if I try to place anything in the queue the program crashes.Configuration: Generated Initialization Place item in queue (btn.dec is a uint8_t variable) Debug As you can see the item size i...

tarmogr_1-1715164215219.png tarmogr_2-1715164240241.png tarmogr_3-1715164262270.png tarmogr_4-1715164307685.png
tarmogr by Associate III
  • 4390 Views
  • 7 replies
  • 1 kudos

headless-build.sh fails in Jenkins

I have managed to run headless-build.sh on my Linux PC. But it requires me to name the project folder exactly the same as the project name. For example /home/user/workspace/freertos-test/freertos-test.iocNow I want to do the build automatically from ...

Resolved! Using Tracealyzer in streaming mode with ST-Link V3

I'm currently testing Tracealyzer but I'm having problems in using it in streaming mode. I followed the indications in video "Visual trace diagnostics with STLINK-V3, Percepio Tracealyzer and DevAlert" (https://www.youtube.com/watch?v=rZlSuq7TySA) to...

paolog by Senior
  • 3351 Views
  • 2 replies
  • 3 kudos

Adding external GCC libraries to STM32Cube project

Hi,I was looking on some tutorials to do FFT on the NUCLEO-L476RG board, where they recomended using CMSIS DSP library. The DSP configuration guide from ST (link below) said to add the library path under Project Properties ->Tool Settings ->GCC Linke...

0693W00000QLEWvQAP.png
NRasm.1 by Associate II
  • 6267 Views
  • 7 replies
  • 0 kudos

Resolved! FDCAN setup on Riverdi display STM32H757XIH6

Hi everyone,I bought a display Riverdi display (RVT70HSSNWC00-B) with a STM32H757XIH6 microcontroller.I want to setup the FDCAN but without success.Has anybody already done and could send a sample ?Thank you in advance.

Can't flash STM32H735IG discovery kit using S32CubeIDE

Hello all,We are trying to evaluate the STM32H735IG for our product. We bought the off-the-shelf dev kit and tried flashing it using S32CubeIDE, but encountered an error. The weird thing is, I can use S32 programmer to read flash, so the ST-Link seem...

Resolved! HTTP web server handling in NUCLEO-F439ZI

Hi team.I develop a code, employs read the ADC value from the LDR and transmit the ADC value serially by UART, and glow the LED if LDR value goes above 1400. It is work fine up to hardware level. Now I update the value in the HTML page using Ethernet...

Ramachandran1992_0-1716266282993.png

Resolved! No ST-Link Detected

I want to program my STM32WB55VG-Q6, but have been getting 'No ST-Link Detected'. I was using a Nucleo board previously and the ST-Link works fine with it. I am able to debug and flash the program onto the Nucleo but not on the STM32WB55VG-Q6 board. ...

lana5_0-1716803656849.png
lana5 by Associate
  • 1900 Views
  • 3 replies
  • 1 kudos

memory usage in stm32

Hi community!I write a simple code in stm32 and I need to calculate the memory usage from the build analyzer this is a part of the code   #define N 16146 volatile uint16_t adc_buffer[N]; int main(void) { HAL_Init(); SystemClock_Config(); MX_GPIO_Init...

toufik_iddou_0-1716736493013.png toufik_iddou_1-1716736558438.png