STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How to switch MCU by CubeIDE?

Hi,When I used CubeMX, MCU could be switched to select[Pinout]→[List pinout compatible MCUs]→[OK, Import]However, in case of CubeIDE, the [OK, Import] button is not appeared.Is the "switch MCU function" deleted?Thanks your help,   

import button.png
Mori1 by Associate
  • 2084 Views
  • 1 replies
  • 1 kudos

Single Conversion Mode for Multi-channel Reading

I m using an STM32 Nucleo F334R8 (for the first time) to control an Inverter. i m having problmes with the ADC channels reading. I have 6 ADC1 channel and 2 ADC2 channels. these channels are going to serve the following purposes:1. All the channels h...

johnjones by Associate II
  • 3959 Views
  • 3 replies
  • 0 kudos

Issue with populating the framebuffer?

So I'm using an ST7789VI display connected to a STM32L4R9I-DISCO board. I've made some test projects in CubeIDE without using TouchGFX to ensure that the driver file and everything else was correct. However, when I try to integrate TouchGFX designs, ...

Hafez1 by Associate III
  • 974 Views
  • 0 replies
  • 0 kudos

Resolved! invalid initializer error

Hello,My first time posting on this forum so apologies in advance. I am working with an LCD screen that will have multiple menu's so I designed this struct with multiple pointers. However, I am running into this error where I cannot seem to use mallo...

msalaz03_0-1721930555970.png
msalaz03 by Associate
  • 3590 Views
  • 3 replies
  • 1 kudos

Resolved! Can't get Printf to work on CubeIDE

Currently using a STM32L4R9I-DISCO and I've been struggling to get the SWV ITNM Data Console to work so I can do some debugging. I'm quite new to this, but I've followed every tutorial online to enable UART and how to set it all up, to no avail. I've...

Hafez1 by Associate III
  • 10599 Views
  • 13 replies
  • 5 kudos