STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1488 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 571 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Can't import a project

Hi All,I upgraded from 1.13.2 to 1.17.0 this week and have created one new project since, in the same workspace as all the ones I have created using the old version. For reasons I won't bore you with I needed to do a re-install of the software today,...

Nucleo-L496ZG-P Issue flashing board

For the first week of having the board, I was able to load different programs with no problem. Somehow, it seems that I got the board into a bad state.  Now, most of the times when I try to flash a program to the board I get the infamous:  Waiting fo...

cbarb2747 by Associate III
  • 3260 Views
  • 10 replies
  • 1 kudos

Why is STM32CubeIDE search so bad? EDIT: Mee bad... sry

EDIT:  Found the search/replace window on a different monitor.  Is there some reason why searching in CubeIDE is so hard to do?  Half the time I hit Ctrl-F (like it says in the File menu) and nothing happens.  I have to read past forum posts to find ...

st3ph3n by Associate II
  • 960 Views
  • 4 replies
  • 0 kudos

Resolved! Signal Pass through using ADC and DAC

The equipment I am using is the following: Nucleo-Board L476RG, STM32CubeIde 1.10.1. I am attempting to design a simple dsp system that uses an ADC to send the data it receives from a function waveform generator to a DAC, and the DAC output will then...

JEscu.2 by Associate II
  • 6175 Views
  • 7 replies
  • 0 kudos

Refresh files to compile after prebuild steps

I run my python script in C/C++ Build --> Settings --> Build Steps --> Pre-build steps by running command:cd ${ProjDirPath}/menu_language_generator && python generate.pyThis script generates header files to my project with langauge translations. Scri...

DBrau.2 by Associate III
  • 1477 Views
  • 2 replies
  • 0 kudos

"Dwarf Error" error after new installation

 Hello friends, thank you for your help.My main problem is that none of the new projects I open on my newly installed STM32Cube on my computer work, but when I import my old projects, they work.part number: stm32f103c8 Environment: STM32CubeIDE / Ver...

WhatsApp Image 2025-02-26 at 11.39.14.jpeg PROG.PNG ERROR.PNG pac.PNG
Sözde.11 by Associate II
  • 1642 Views
  • 2 replies
  • 0 kudos