STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1417 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Debug a Zephyr project in STM32CubeIDE - Windows

Hi All,I'm trying to setup STM32CudeIDE 1.17.0 to build and debug my Zephyr OS project (STM32H745).  Mainly to get access to the dual core debugging features that the IDE provides.I found Zephyr has a page to guide setup on a Linux machine, but the s...

Simon33rd_0-1737015528712.png
Simon33rd by Associate II
  • 1962 Views
  • 2 replies
  • 0 kudos

STM32 package installation error

Hi,I have recently installed STM32CubeIDE 1.18.0 on my windows 11 pc. I am not able to generate the code using a .ioc file. I always get package installation failure error as show below in the imageWhy is this error happening and how can I resolve th...

avbST_0-1744112403416.png
avbST by Associate II
  • 1236 Views
  • 2 replies
  • 0 kudos

Resolved! STM32C0116-DK default project shows configuration warnings

I installed Cube 1.18.1 and selected STM32C0116-DK (STM32C0xx eval board) and created a test project. But when I open the .ioc file to check hw config I can see that there are warning signs on ADC1, TMR1, TMR3 and USART1. I disable SPI1 and USART2 bu...

MWebj by Associate III
  • 1904 Views
  • 5 replies
  • 1 kudos

STM32H7 freeRTOS heap_4 condition

Hi. Previous (in stm32u5), I used to select X-CUBE-FREERTOS and inside that you could select heap version. (heap_5, heap_4, ...) and that heap version selection would satisfy another component that had dependency on heap_4 (or other versions.).But in...

miladmohtashamirad_0-1744776014885.png

STM32H7S78-DK - Error: failed to erase memory

I am using STM32CubeIDE to program my board i.e. STM32H7S78-DK. My file size is in large due to which it is flashing in external flash at address 0x70000000. In case of smaller file size i.e. less than 64 KB, it flashes in internal flash at address 0...