2025-04-16 10:22 PM - edited 2025-04-16 10:23 PM
Hello,
I'm trying to silently install Atollic TrueSTUDIO for STM32 v9.3.0 for use in a CI/CD pipeline.
I'm launching the installer from a .bat file using the following command:
Atollic_TrueSTUDIO_for_STM32_windows_x86_v9.3.0_20190212-0734.exe /S /D=C:\Tools\TrueSTUDIO
Were:
/S = Silent installation (commonly used with NSIS-based installers)
/D= = Destination path for installation
The installation does not run in silent mode – the graphical installer still appears. There are no error messages, but also no indication that a background installation is taking place.
Does the TrueSTUDIO installer support silent installation at all?
Setup Details:
TrueSTUDIO Version: 9.3.0 (Build 20190212-0734)
Platform: Windows 11
Installer Filename: Atollic_TrueSTUDIO_for_STM32_windows_x86_v9.3.0_20190212-0734.exe
Any insights or suggestions would be greatly appreciated – thanks in advance!
Martin
Solved! Go to Solution.
2025-04-28 6:31 AM
Hi everyone,
just a quick update in case anyone faces a similar challenge:
I manually installed TrueSTUDIO once, then simply zipped the installation directory and now use that archive in our CI/CD environment.
Of course, it's not a "clean" solution, but for our legacy use case, it works reliably.
Maybe this pragmatic approach will help someone else as well.
Best regards,
Martin
2025-04-17 4:19 AM
Silent install is an option with NSIS, not a standard. However, I would like to point out that Atollic Truestudio has Not been Recommended for New Developments (NRND) for a very long time. Due to the outdated database of supported MCUs alone, the constantly updated STM32CubeIDE should be used instead.
Regards
/Peter
2025-04-17 4:38 AM
Hi Peter,
Thanks for your response – and yes, I'm aware that Atollic TrueSTUDIO is not recommended for new designs and no longer recommended for new developments. In this particular case, however, we're maintaining a legacy toolchain for an existing setup, and for that reason, TrueSTUDIO is still required.
That's why I'm specifically interested in whether a silent installation is possible with the provided Windows .exe installer – even though it's an older setup.
Best regards,
Martin
2025-04-28 6:31 AM
Hi everyone,
just a quick update in case anyone faces a similar challenge:
I manually installed TrueSTUDIO once, then simply zipped the installation directory and now use that archive in our CI/CD environment.
Of course, it's not a "clean" solution, but for our legacy use case, it works reliably.
Maybe this pragmatic approach will help someone else as well.
Best regards,
Martin