NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi.I'm working with the EVAL STM32WB5MM-DK for a while now, already programmed the stack and the FUS many times, and it's the first time I got this error.After successfully open STM32CubeProgrammer (v2.19) and connected to the programmer, Selecting t...
There are already a few threads discussing this topic, but none of them have an answer.How can one force the STM32WB35 to send an event upon receiving a scan request? The documentation (rather vaguely) states that this can be achieved by setting the ...
Hey there,i have a custom board designed which is broadcasting stuff over BLE.So far i am using the full_stack_fw which works quite well.In order to turn on extended advertising i wanted to switch over to the full_extended_stack (needed for extended ...
I created the OTA application by following this YouTube video:https://www.youtube.com/watch?v=mRzZOa3jmuM&list=PLnMKNibPkDnG9JRe2fbOOpVpWY7E4WbJ-&index=14https://www.youtube.com/watch?v=mRzZOa3jmuM&list=PLnMKNibPkDnG9JRe2fbOOpVpWY7E4WbJ-&index=13Afte...
Hi, I'm having a problem with the wake-up procces using interruptions. I use three pins, PA0, PA8 and PA9, set the with no pull-up, and in rising mode. then i enable them as wake up pins, in rising mode. i go to sleep in stop mode, using the function...
Hello Team,I am currently working on STM32WLE5 microcontroller and getting issue in HAL_Delay(), it got stuck, ifound that systick interrupt was not generating. In main() function, I start with HAL_Init() and then HAL_Delay(500) and controller get st...
Hi,I was going through the documentation in this link. It mentions that there is a transparent mode. How can I enable this in the example for PBP Source?/* Codec Mode */ typedef uint8_t CODEC_Mode_t; #define CODEC_MODE_DEFAULT (CODEC_MODE_FLOW_C...
I am implementing a dual-firmware architecture on an STM32 microcontroller that does not natively support dual-bank flash. In this setup, I have partitioned the internal flash memory into two separate blocks:Block 1 (Bootloader + Application) begins ...
I've a custom board that going to SHUTDOWN OFF mode I'm using the LPM lib and it use PA0 as WAKEUP PIN it wakes up on a High level signal void PWR_EnterOffMode(void) { /* USER CODE BEGIN PWR_EnterOffMode_1 */ // refer to the following link for more...
Hello.I found a problem with Flash. After successfully operating with flash before entering MX_APPE_Process(), the possibility of entering standby mode disappears. I had issues with the visibility of variable values after these operations, but I coul...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.