User Activity

Hi, We are trying to write some key values directly into a particular address of NVM from STM32Cubeprogrammer, but rest of the sector are also getting erased. Is there any way to prevent it? Tested with Cubeprogrammer CLI also, but facing the same is...
Hi,In RAK3172 which have STM32WLE5CCU6, during the flashing of DEVEUI,JOINEUI ,APPKEY and NWKKEY in which memory location of NVM this values are being stored. Is there any documentation for same? Also can we flash these keys directly to NVM using STM...
Originally a reply in this old thread: https://community.st.com/t5/stm32-mcus-wireless/not-able-to-disable-receiving-window-of-l072z-lrwan1/m-p/657145@Andrew Neil Sorry for Newbie question, so let's say I want to keep the rx window(in class C) open f...
What are the differences between LPTIM and TIM, also doesTIM1,TIM2,TIM16,TIM17 work when the device is in STOP2 mode?
Hello, I have a RAK3172 which is based on STM32WLE5CCU6, and it is being configured for LoRaWAN, and the node transmission is happening based on timer (TX_ON_TIMER), sometimes an External interrupt will be there and the device needs to send the packe...
Kudos given to