NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Posted on December 25, 2017 at 06:38Hello everyone,I am using Murata LoRa discovery board DISCO-072CZ-LRWAN. A simple queryWhen I put the STM32L072CZ (present in the board) to sleep, does that mean the SX1276 LoRa trans receiver also goes to sleep? ...
Posted on December 23, 2017 at 14:51Hello everyone,I have a general query about any embedded system. Whenever we use any communication device(maybe Bluetooth or WiFi or GSM), is it advised to use AT commands to control the device?Thank you in advanc...
Posted on December 22, 2017 at 06:36if is it possible then which memory are use for store the hex file.external flash or system flash?please suggest other option also.
Posted on December 19, 2017 at 15:26I have two queries for anyone who can help me,1)What is the maximum payload for US915_HYBRID, SF7, 125kHz BW for LoRa?2)I need an extra UART on stm32l072cz LoRa discovery board. Can anyone help with this.Please he...
Posted on December 15, 2017 at 15:42I am a beginner on stm32 microcontroller I am currently using Nucleo-L073RZ I am wondering if there is any code examples may help me to understand how to recieve data via Uart (TX,RX) and send it via Lora Network...
Posted on December 16, 2017 at 05:53Hello everyone, this is a problem regarding my DISCO-L072CZ-LRWAN kit which I am using for a project of mine.I am using the LRWAN expansion kit for LoRa functionality while I am also trying to add up a UART as UAR...
Posted on May 03, 2017 at 11:42Does anyone have any experience with the current consumption when using B-L072Z-LRWAN1 (STM32L072 and LoRa board) with i-cube-lrwan 110?I can't get the current consumption below below 1.1mA no matter what i try. In low...
Posted on October 30, 2017 at 17:25 Is it possible to 'manually' configure the Tx Power level using theI-CUBE-LRWAN v1.1.2 software? I can see that the End_Node demo enables Adaptive Data Rate: /* ! *Initialises the Lora Parameters */ sta...
Posted on September 15, 2017 at 16:29Hi All,I am using STM32l073 nucleo board with module. I am unable to get power more than 14.6 dBm while transmitting data packet. On my other device i am able to get 19 dbm of power using same sx1272 module.I tri...
Posted on December 01, 2017 at 05:42Hi All, I have a custom designed PCB with STM32L073RZ + SX1276 LoRa transceiver + LIS2DH12 MEMS accelerometer. LoRa chip uses SPI2 and sensor uses SPI1 interfaces. Interrupts for the sensor are not being used. The...