NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi!I have used the B-L072Z-LRWAN1 with the module CMWX1ZZABZ-091. I used the software from I-CUBE-LRWAN and it worked correctly. But now I am trying to test the module CMWX1ZZABZ-078 with the same software (the example of AT_slave). The communication...
Hi,I'm flashing the CMWX1ZZABZ LoRa module (STM32L082) for the first time. I have JLink ARM Lite debugger. I connected to SWDIO, SWCLK, nRST and GND pins to the JLink debugger. But when I try to flash/erase the memory, it a message saying "***JLink E...
Hi STM,I am relatively new to the embedded (I have decent C++ background). So my question revolves around start exploring STM. My idea is to start with Nucleo board and some Wi-Fi expansion board. Can you, please advice what would proper combination ...
HAL_UART_Receive(&huart2, (uint8_t*)msgToTransmit, MESSAGE_SIZE, HAL_MAX_DELAY); int index = 0; for (index = 0; index < MESSAGE_SIZE; index++) { PRINTF("\n\rmsg to transmit is hex: %x", msgToTransmit[index]); PRINTF("\n\rmsg to transmit is c...
Hi,I have STM32L4A6VGTx with SPWF04SA wifi module on it. I want to send sensor data to Amazon IoT. I can see AT+S.TLSCERT commands for the wifi module. I have created a thing on Amazon IoT core and I have downloaded certificiates (myrootCA1.pem, myce...
Hello, when will the STM32WB55CB and the STM32WB nucleoboards be released? Is there any approximate timeline?
Hello ,I use this demo board B-L072Z-LRWAN1 with the soft End Node I-CUBE-LRWAN 1.2.0But I do not understand why I cant send the messagei disable all senser and i try to send with " LORA_send( &AppData, LORAWAN_DEFAULT_CONFIRM_MSG_STATE); "in static ...