Hi, it seems that the STEVAL-WLC38RX uses STSW-WPSTUDIO and the STEVAL-WBC2TX50 uses STEVAL-WBC2TX50. Is it possible to program the STEVAL-WLC38RX to take external ADC measurements via the NTC pin or the GPIOs and send it to the STEVAL-WBC2TX50 using...
I am trying to use mbed to send AT Commands to the SPBT3.0DP2 module in order to change it's baud rate. I am using the ATCmdParser to send the AT commands. It seems like I am not able to enter the command mode? I'm not sure. please help.I do at.send(...
Hello, I was wondering if there are plans to make another stm32wb series chip with an internal DAC and maybe some op-amps. Also, will they make nucleoboards for these chips?
Hi,Thanks for the prompt response. Yes, I meant that I want to send send RX NTC data to TX/STWBC2. However I am curious if:1) The STWLC38 can be programmed to autonomously measure and send RX NTC to TX/STWBC2 data at a fixed interval?2) If the STWBC2...