NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,I am using B-L072Z-LRWAN1 and I-Cube-LORAWAN SDK specifically AT_Slave project. I am trying to put device in Stop mode but I can see it exist from stop mode immediately.How can I put some condition for device to exit from stop mode or not? Are th...
Hello to all, Im new here I have two B-L072Z-LRWAN1 discovery board. Installed board support package from https://github.com/GrumpyOldPizza/ArduinoCore-stm32l0 I can able to program 1board using arduino ide but when i try to upload on 2nd Board it...
Hello,When running the example code for the B-L072Z-LRWAN1 module STM32CubeExpansion_LRWAN_V1.2.0 i have an extremely high run current. I added some user code running an algorithm which needs some seconds to terminate. The measured current during MCU...
Hi,I am using B-L072Z-LRWAN1 and AT_Slave project from I-Cube-LRWAN. Can Anyone help me with the setup to measure current consumption like jumper position and across which pins to measure current?Thank You
Please help me with:OS_1:Arch Linux(64)Atollic TrueSTUDIO 9.3OS_2:Windows 7(64)Atollic TrueSTUDIO 9.3en.x-cube-sfox.zip project was taken:https://www.st.com/en/embedded-software ... -sfox.htmlFor bulding example project:STM32CubeExpansion_SFOX_V1.1.0...
Hello All,I'm planing to use a STM32WB55C on a design and I have the choice to either use an old-fashioned Pi matching network + Filter or use an integrated MN/Filter (MPLF-WB55-01E3).Knowing that the part have 0 stock (some expected in a few weeks o...
Hello,Concerning the AN3359, what is the unit of the figure 2 ?Thanks.
STM32CubeWB is the firmware package of the stm32wb series.when i clicked the Get Software Button,the page jumped to the home page.I have logged in to my ST Account.
GSM modem is attached to STM32. Using FTP AT commands I am able to download a particular file from FTP server. Now I don't know where this downloaded file is saved inside the GSM modem. My goal is to transfer that file into STM32 and upgrade the firm...
Hi,I am trying to evaluate Thread connectivity with my brand new STM32WB development kit using Thread_Cli_Cmd example. I connect the board NUCLEO-WB55.Nucleo to my PC via the ST-LINK connector then I run STM32Cubeprogrammer, did a full chip erase and...