What does AT+CERTIF command? (AT commands in I-CUBE-LRWAN for FCC certification)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-08-15 11:58 AM
Hello,
We designed a device with CMWX1ZZABZ-091 LoRa module on I-CUBE-LPWAN (Our FW is based on AT_Slave example).
Now we are in the middle of getting FCC certification and our certification lab asked us to provide a command for testing radio.
We recommended them to use AT+TTLRA command every time they need to send a packet, but it seems that they are not able to select a specific freq/channel to transmit on.
The only option they have is to select 868 or 915 MHz using AT+TCONF command.
We also found AT+CERTIF command but do not know what exactly it does. Can you describe it?
And maybe there is another AT command we can use for testing radio (transmitting on a specific channel for testing all channels separately)?
Thanks in advance!
- Labels:
-
LoRa