STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! Is there a simple way to turn BLE off and on?

I would like to be able to turn BLE off (e.g. with a timer) even if it is currently connected. I know I can stop it advertising, but this doesn't seem to kill the connection. Basically, after a timeout, I would like the BEL to shutdown and stop using...

AClif by Associate III
  • 2473 Views
  • 2 replies
  • 0 kudos

Problem with HAL_Delay while using PWM+DMA in STM32WB55

Hello! I am using PWM to generate 1.25 ms period pulse to trigger a LED strip light . In main.c , properly in while(1) when I called HAL_TIM_PWM_Start_DMA followed by HAL_Delay the program got stuck in uint32_t tickstart = HAL_GetTick(); . When I run...

0693W000001syBGQAY.png
Kolab by Senior
  • 2214 Views
  • 4 replies
  • 0 kudos

Can the STM32WB55 OTA handle encrypted user applications?

As far as I understand, the OTA example provided (BLE_Ota) supports either flashing the user application directly or handing the processing over to CPU2 for decryption of the Wireless firmware (which comes as an encrypted and signed package).Is it po...

HRadt.1 by Senior
  • 2368 Views
  • 5 replies
  • 0 kudos

I2C error handling.

I am using the following code:  while(HAL_I2C_Master_Transmit(&hi2c1, DEVICE_ADDR, i2cbuffer, 1, 1000) != HAL_OK)  {   /* Error_Handler() function is called when Timeout error occurs.     When Acknowledge failure occurs (Slave doesn't acknowledge its...

BMart.2 by Associate II
  • 3748 Views
  • 1 replies
  • 0 kudos

I2C Error Trapping

I am using the STM32WB in master mode, polling a single LSM303AGR accelerometer. Using the HAL transmit routine as follows:if(hi2c1.State == HAL_I2C_STATE_READY) {  /* Now send the device address and register to be read with 1 sec delay max*/  while(...

0693W000001sxN6QAI.png
BMart.2 by Associate II
  • 1228 Views
  • 1 replies
  • 0 kudos

I2C Error Trapping

I2C Error trappingI am using the STM32WB in master mode, polling a single LSM303AGR accelerometer. Using the HAL transmit routine as follows:if(hi2c1.State == HAL_I2C_STATE_READY) {  /* Now send the device address and register to be read with 1 sec d...

0693W000001sxN6QAI.png
BMart.2 by Associate II
  • 3061 Views
  • 1 replies
  • 0 kudos