STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 228 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4071 Views
  • 0 replies
  • 3 kudos

Resolved! Trying for 2_Images_UserApp with STM32WL55 Nucleo-64 but seems I'm not able to link the User App for CM0+ core. The linker is specifying that several symbols have been already defined elsewere.

Further investigating I see that the problem seems related to symbols exported for the se_interface, compiled into the 2_Images_SBSFU_CM0PLUS project and exported as .elf and .o file, thus included in the 2_Images_UserA__CM0PLUS project linking phase...

0693W000008wdl9QAA.jpg
MSign.1 by Associate II
  • 1285 Views
  • 1 replies
  • 0 kudos

MB1720- LORA

Hi ,We have designed the custom PCB based on "MB1720", tried the LORAWAN_end_node example on our custom board. but there is no signal out from RF antenna. do we need to modify anything related to MB1720? We have the NUCLIO-WL55JC devboard, the same i...

MSai by Associate II
  • 1568 Views
  • 2 replies
  • 0 kudos

Starter pack delivery

Hi, is it possible to provide me with a tracking number to see when the p-nucleo-lrwan and wl55jc devkits will be delivered? I'm booked for the session on the 19th of March

CLind.1 by Associate II
  • 1072 Views
  • 2 replies
  • 0 kudos

BLUENRG-M2SA: I have been tasked with a prelim investigation into a new product - battery powered BT device. Will communicate with app on phone to receive data to control LED interval used for alarms

M2SA or M2SP device looks promising. What isn't clear to me is if this module needs to interact with a separate micro for my program? or is there room for my program in this module? I am trying to do an energy analysis.

GGibb.1 by Associate II
  • 804 Views
  • 0 replies
  • 0 kudos

Latencies / Buffer sizes of FP-AUD-BVLINKWB1?

So I am trying to synchronize microphones with a clap board; that works nicely as-is but when I tried to change the N_MS_PER_INTERRUPT to 10 (on both BVOPUS_PER and BVOPUS_CEN), I get clicks in my audio signal.I've changedN_MS_PER_INTERRUPTAUDIO_OUT_...

TJohn.14 by Associate II
  • 1829 Views
  • 1 replies
  • 1 kudos

STM32WB5MMG OTA using IAP over LTE CAT-M1/GSM using HTTP/S

Hi community,I like to make my life a bit more difficult than necessary.Using a Quectel modem, connected via USART to the STM32WB5MMG, I want to enable OTA upgradeability over LTE CAT-M1/GSM. The downloading part is already figured out from older pro...

CKnez.1 by Associate II
  • 1083 Views
  • 0 replies
  • 1 kudos

Beginner's question: Can't get ITM/SWO to work

I am doing my first steps on the NUCLEO-WL55JC1 and one of the first things I like to get working is of course some debug printfs. Though I could of course use the VCP via the integrated STLink I'd like to use ITM_SendChar() to output some informtion...

MDaub.1 by Associate III
  • 4772 Views
  • 2 replies
  • 1 kudos