User Activity

Hi,According to the datasheet I must supply 3.3V to VDDUSB when USB is in use, but my question is - Can I connect 3.3V LDO directly to VBUS, so that when USB is not present - USBVDD pin is 0V. Its is unclear whether this works from the datasheet. In ...
It asks to re-connect STLINK and press "yes". Nothing happens after. I've tried to install STM32CubeProgrammer to upgrade manually, but I could not get it running.OS X 10.15.4 java 14.0.1 2020-04-14Java(TM) SE Runtime Environment (build 14.0.1+7)What...