cancel
Showing results for 
Search instead for 
Did you mean: 

I have a simple code to run a webserver that toggles LED on STM32 Nucleo. I connect to WiFi using ESP 8266 which works perfectly well. I want to migrate this code to Sensortile which uses STM32 L476JGY. using ESP8266. It doesn't work. How do I do it ?

ABhaw.1
Associate

I follow the exact same procedure. I generate code, set GPIO and clock in Cube MX. Open the file in System Workbench. Initialize all the pins right.

I should be connecting the ESP8266 pins to the expansion board right ? This expansion board is connected to the nucleo using the SWD connector.

I feel like I'm missing a step. I ran the example data logger project which works fine on the sensortile.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0