STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! STM32L010K8 ROM Bootloader via I2C

Hello, I have a wearable design which consists of 2x STM32 MCUs (One STM32WB and a STM32L010K8). They are connected via I2C and I need to be able to reprogram the STM32L010K8 using the STM32WB via the I2C port. However, there's mixed information rela...

DCamp.4 by Associate II
  • 2983 Views
  • 8 replies
  • 0 kudos

Resolved! How do you install WB RF stack?

Hi. I've read several bits of info on the RF stack installation, but can't figure it out. Here's a previous thread on the topic:https://community.st.com/s/question/0D53W00000DKLKkSAP/how-do-i-flashburn-the-ble-stack-coprocessor-binary-for-my-stm32wb5...

DOCon.1 by Senior
  • 1694 Views
  • 4 replies
  • 0 kudos

Is it possible to use dfu bootloader with the stm32wl55 device

I’am working with the stm32wl55 device, now I’am looking how can I update my firmware. I’d like to use dfu bootloader but after reading AN2606 note only USART and SPI bootloader mode are available for stm32wl55, so dfu isn’t available ? And I’am also...

SBaro.11 by Associate III
  • 1176 Views
  • 2 replies
  • 0 kudos

Resolved! LRWAN_V2.0.0 PingPong doesn't work.

I'm using NUCLEO_L073RZ with LRWAN NS1 which included in P-NUCLEO LRWAN 3.​I tried to communicate two end devices with SubGhz_Phy project in STM32CubeExpansion_LRWAN_V2.0.0, but it doesn't work.It seems to using SPI, but MOSI(PA7) and MISO(PA6) is co...

CKim.8 by Associate
  • 1542 Views
  • 3 replies
  • 0 kudos

STM32WLE5JC VREFBUFF Internal Reference

I am trying to use the internal voltage reference on the STM32WL MCU. When I enable the VREBUFF, it always times out and the VREFBUF->VRR bit is not ready.On other STM32 MCU family, I read that it is required to enable the clock for SYSCFG and VREFBU...

HDaou by Associate
  • 1284 Views
  • 1 replies
  • 0 kudos