cancel
Showing results for 
Search instead for 
Did you mean: 

Smart wearable recommendation?

程张.1
Associate

智能穿戴产�?带�?牙5.0的芯片有没有推�??的?

�?牙芯片 [�?制链接]

这个�?牙芯片我们希望集�?更多的功能,比如内存有1M以上;有ADC采样,有OP�?放,或者内置有AFE电路;有充电管�?�(如果没有�?�以增加充电芯片,本身充电芯片体积�?会很大);需�?5.0或以上版本;带电�?监测功能或者�?�以外挂电�?计芯片;有串�?�或者IIC接�?�;这样的过功能�?牙芯片有没有�?�适的或者接近的?类似一个SOC的功能

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Ulysses HERNIOSUS
ST Employee

Google translation as:

Is there any recommendation for smart wearable products with Bluetooth 5.0 chips?

Bluetooth chip [Copy link]

We hope to integrate more functions of this Bluetooth chip, such as memory with more than 1M; ADC sampling, OP amplifier, or built-in AFE circuit; charging management (if there is no charging chip can be added, the size of the charging chip will not be very large Large); version 5.0 or above is required; with current monitoring function or an external fuel gauge chip; with serial port or IIC interface; is there such an over-function Bluetooth chip that is suitable or close? Similar to a SOC function

程张.1
Associate

看�?懂 都是英文�?�​

Hi,

General language of this community is English. If you want to successfully participate (receive answers) I recommend to use English. Maybe you can use translation service like Google translate.

-- Google Translate -->

这个社区的通用语言是英语。 如果你想�?功�?�与(收到答案)我建议使用英语。 也许你�?�以使用�?谷歌翻译这样的翻译�?务。

此致

Best Regards, Ulysses