2021-06-02 1:37 AM
Can anyone tell me what Update_Type parameter does in this fucntion?
tBleStatus aci_gatt_update_char_value_ext( uint16_t Conn_Handle_To_Notify,
uint16_t Service_Handle,
uint16_t Char_Handle,
uint8_t Update_Type, // -------> What values can it get? What does it do?
uint16_t Char_Length,
uint16_t Value_Offset,
uint8_t Value_Length,
const uint8_t* Value )
Is there any description documentation regarding the hci BLE messaging to BLE side?
Thansk?
Solved! Go to Solution.
2021-06-09 2:04 PM
Check out the header file that contains the prototype, it explains the options.
/**
* @brief ACI_GATT_UPDATE_CHAR_VALUE_EXT
* This command is a more flexible version of ACI_GATT_UPDATE_CHAR_VALUE to
* support update of long attribute up to 512 bytes and indicate selectively
* the generation of Indication/Notification.
*
* @param Conn_Handle_To_Notify Connection handle to notify. Notify all
* subscribed clients if equal to 0x0000
* @param Service_Handle Handle of service to which the characteristic belongs
* @param Char_Handle Handle of the characteristic declaration
* @param Update_Type Allow Notification or Indication generation,
* if enabled in the client characteristic configuration descriptor
* Flags:
* - 0x00: Do not notify
* - 0x01: Notification
* - 0x02: Indication
* @param Char_Length Total length of the characteristic value.
* In case of a variable size characteristic, this field specifies the
* new length of the characteristic value after the update; in case of
* fixed length characteristic this field is ignored.
* @param Value_Offset The offset from which the attribute value has to be
* updated.
* @param Value_Length Length of the Value parameter in octets
* @param Value Updated characteristic value
* @return Value indicating success or error code.
*/
tBleStatus aci_gatt_update_char_value_ext( uint16_t Conn_Handle_To_Notify,
uint16_t Service_Handle,
uint16_t Char_Handle,
uint8_t Update_Type,
uint16_t Char_Length,
uint16_t Value_Offset,
uint8_t Value_Length,
const uint8_t* Value );
2021-06-09 2:04 PM
Check out the header file that contains the prototype, it explains the options.
/**
* @brief ACI_GATT_UPDATE_CHAR_VALUE_EXT
* This command is a more flexible version of ACI_GATT_UPDATE_CHAR_VALUE to
* support update of long attribute up to 512 bytes and indicate selectively
* the generation of Indication/Notification.
*
* @param Conn_Handle_To_Notify Connection handle to notify. Notify all
* subscribed clients if equal to 0x0000
* @param Service_Handle Handle of service to which the characteristic belongs
* @param Char_Handle Handle of the characteristic declaration
* @param Update_Type Allow Notification or Indication generation,
* if enabled in the client characteristic configuration descriptor
* Flags:
* - 0x00: Do not notify
* - 0x01: Notification
* - 0x02: Indication
* @param Char_Length Total length of the characteristic value.
* In case of a variable size characteristic, this field specifies the
* new length of the characteristic value after the update; in case of
* fixed length characteristic this field is ignored.
* @param Value_Offset The offset from which the attribute value has to be
* updated.
* @param Value_Length Length of the Value parameter in octets
* @param Value Updated characteristic value
* @return Value indicating success or error code.
*/
tBleStatus aci_gatt_update_char_value_ext( uint16_t Conn_Handle_To_Notify,
uint16_t Service_Handle,
uint16_t Char_Handle,
uint8_t Update_Type,
uint16_t Char_Length,
uint16_t Value_Offset,
uint8_t Value_Length,
const uint8_t* Value );
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.