STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 142 Views
  • 0 replies
  • 0 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4033 Views
  • 0 replies
  • 3 kudos

B-WL5M-SUBG1 Power consumption measurement

Hi All,I am working on B-WL5M-SUBG1 hardware.I compiled the example "C:\...........\STM32Cube\Repository\STM32Cube_FW_WL_V1.3.0\Projects\NUCLEO-WL55JC\Examples\PWR\PWR_STANDBY" to  measure the current consummed in standby mode and I am measuring the ...

STeng by Associate
  • 1291 Views
  • 2 replies
  • 1 kudos

Can't transmit data with LoRa

Hi everyone,I have custom stm32wle board that is configured as dc-dc supply, and external 32MHz crystal with 6.8pF capacitors.I can read and write to/from radio registers but i can't transmit any data. Indeed even transmit interrupt (HAL_SUBGHZ_TxCpl...

krf by Associate II
  • 469 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WB55 ADC Internal Resistance Issue

Hello STM Community,I’m currently working on measuring a LiPo battery voltage using one of the ADC inputs (AIN6) on an STM32WB55RG. The battery voltage ranges from approximately 3.0 V to 3.95 V. Since the ADC reference (Vref) is 3.3 V, I used a volta...

Resolved! LoRaWAN Software Stack for STM32WLE5xx

How I get the software stack/firmware library stack with LoRaWAN for STM32WLE5xx MCU (other than Seed Studio Library) ?. In github, stm32wl repository only has a STM32WL55JC drivers alone. Is there any possibilities to get a firmware stack for STM32W...

Sequencer stop when LPTIM1 Started

I am using the LoRaWAN_End_node application.  The application was working fine until I integrated the Low Power sample code.  The Sequencer appears to stop working (I suspect the timers are not working).  If I do not do add MX_LPTIM1_Init() in main e...

jlaiosa by Associate II
  • 427 Views
  • 2 replies
  • 0 kudos

STM32WBCEU6 BLE ISSUE

Hi all,I am using the STM32WB55CEU6 to share data using BLE technology. I have designed a customized PCB based on my requirements. I fully configured the STM32CubeIDE .ioc file according to ST’s reference documents. However, I am not getting any outp...

Resolved! STM32WB55 LPUART Baud Rate Issue

 Hello STM Community,I’ve been struggling with an issue for some time and would appreciate your insights.I’m using an STM32WB55 MCU connected to an LTE modem via LPUART for cellular communication. The modem’s default baud rate is 115200.I use a ring ...

kickerkro by Associate II
  • 1067 Views
  • 7 replies
  • 3 kudos