User Activity

I'm creating a new lora project starting from STM32Cube_FW_WL_V1.2.0, application LoRaWAN_SBSFU_1_Slot_DualCore.I reserved some space (from 0x0801A000 to 0x0801BFFF) for some configurations. I modified the file mapping_fwimg.ld like below.\STM32Cube...
I'm working on the application project LoRaWAN_AT_Slave_DualCore from STM32Cube_FW_WL_V1.1.0 .The payload of the downlink messages is not correctly transfered from the processor M0 to the processo M4. There is a bug in:file LmHandler_mbwrapper.c, fun...
Kudos from