NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,My project is SubGHZ Phy Ping Pong. In AN5568 the Rx consumption varies from 4mA to 10mA. In my project, the Rx consumption current from 8mA to 9mA. I want to reduce the Rx consumption. My configure below,Please recommend me some solutions.Thanks.
A new version of STM32CubeMonitor-RF has been released to support the STM32Cube_FW_WB_V1.14.0.Update the 802.15.4 sniffer firmwre and addition of Nucleo sniffer firmware.Alignment of OpenThread API with the firmware delivered in the STM32Cube_FW_WB_V...
Can anyone confirm if it is okay to supply the RF switch directly from a general purpose output of the STM32WL? This way I could control when the switch is working or when the antenna is isolated (off) from the circuit.I see in the datasheet for the ...
CPU1 should only be used to initialize the System, boot CPU2 and then go in Standby permanently. The CPU2 should be programmed to read sensor data for a few minutes and then also go in Standby Mode.When the whole system is in Standby mode, it should ...
The STM32WB55 microcontroller have SMPS internally. Can I use it to convert AC power to DC power for the microcontroller? If possible, I want to supply RF inductive charging power directly to the microcontroller.
Hello!We are developing device on STM32WB55 MCU along with mobile app companion. We use stm32wb5x_BLE_Stack_light_fw. The MCU works as Peripheral, mobile app - as Central.In our firmware we use internal FLASH to store some configurations. Our applica...