STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 220 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WLE RAM Retention Only Functional in Debug Mode

Hi there,I am using an STM32WLE and putting it into Standby mode for extended periods of time. I am trying to retain SRAM2 while in Standby mode, and it is working while the DBGMCU_CR_DBG_STANDBY bit is set. However, when I clear the bit SRAM2 is no ...

RLind.3 by Associate III
  • 2278 Views
  • 3 replies
  • 0 kudos

Resolved! SMPS in STM32WB55 microcontroller

I found that the STM32WB55 microcontroller have SMPS but I cannot understand how much external component is required.Here is basic SMPS circut and could you tell me how much circuit is in the microcontrollers SMPS?

0693W00000QKUdvQAH.png
KKIM.6 by Senior II
  • 2868 Views
  • 4 replies
  • 0 kudos

Hello everyone, I have the flash memory AT25SF321B and I want to write and read it. As a µC I use an STM32WB55. I write some values but if i read it back i get only zeros. But i can read the manufacture id 1F 87 01. Hope you can help me.

// 25AA040A instructions const uint8_t EEPROM_READ = 0x03; // 03h Normal Read Data const uint8_t EEPROM_WRITE = 0x02; // 02h Page Program const uint8_t EEPROM_WRDI = 0x04; // 04h Write Disable const uint8_t EEPROM_WREN =...

0693W00000QKzvlQAD.png 0693W00000QKzwAQAT.png 0693W00000QKzw5QAD.png 0693W00000QKzsUQAT.png

Problems with ZigBee custom cluster

Greetings,Recently I tried to implement a ZigBee custom cluster by taking inspiration from the custom long string cluster.Basically, the client is requesting data by using ZbZclClusterCommandReq and the server is answering thanks to the ZbZclClusterC...

E.C. by Associate II
  • 924 Views
  • 0 replies
  • 0 kudos

Resolved! STM32wb55 HAL_Delay() Function

Hi everyone,I have been stuck at a problem. I have been trying to configure HAL_Delay function to work in STM32 BLE_Server example in the STM32WB SDK. However, for some reason, the code gets stuck inside the HAL_Delay() Function. I have searched over...

AKetc by Associate III
  • 9683 Views
  • 20 replies
  • 1 kudos

Resolved! Why are some Examples/Applications for the nucleo64 (STM32WL55) single core and some dual core, and how can i switch it in my projects?

Hi, newbie here, while browsing the Examples for the NUCLEO-WL55JC1, it came to my attention that some have a dualcore version. The SubGHz_Phy_PinPong for Example.Does one core get disableled in the non dualcore Version? And how can i change the sett...

D.Heink by Associate III
  • 1294 Views
  • 2 replies
  • 0 kudos