NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello everyone,I wonder if it is possible to develop and run a custom coprocessor firmware on the Cortex-M0 of the chip. From what I understood so far, the FLASH and RAM portions dedicated to FUS, Safeboot, and Wireless Stack are locked from the fact...
Hi all,I have my own customized board based on STM32WB55RGV6. The board has HSE of 32 MHZ but don't have LSE. I am using LSI or (HSE/32) as RTC clock and HSE/1024 as RF wakeup clock. I am facing two different problems.Case 1: First I tried with examp...
I've seen that it's support Bluetooth 5.2 which added LE Audio feature.Is it possible to make SSTM32WB55-based sound device (i.e. BLE to 3.5 mm jack converter)?And how if so?
Hello,My firmware sends data to TTN when I double push on the button of my board. When the first push is detected, the board wakes up from low power mode and a timer is launched to detect if there is a second push. At the end of the countdown, if the...
I am using the STM32WB55 Series for my application. I am using BLE and Zigbee on this MCU. I am registering my devices for FDA/CDSCO certification. The department is asking for ETA certificate. DO we have ETA Certificate for Controller?
I already got it: CPU2 is not accessible by customer (at least, using official SDK).Anyway, we have an WB-based project that will hugely benefit from offloading some resource-consuming tasks to CPU2. They are not related to radio, we're not using any...
I'm working with STM32WL and trying to be able to generate PWM signal after wake up from STOP2 to control RGB LED. Before going to STOP2 I deinitialize PWM channel pin and disable timer clock. MCU wakes up on button press. After wake up timer clock i...
Hi,I am using Zegbee messaging cluster on STM32WB55 to send messages between some Zigbee end devices and a coordinator.Each end device measures the temperature via I2C sensor and sends a message with the temperature value to the coordinator and then ...
I had one STM32 debugger (ST-LINK-v2). how to learn the STM32 debugger and how to connect the stm32 chip to the debugger. give any solution or tutorial.I will be waiting for your replays. Thank you.
If I call SUBGRF_SetRx() with a timeout of, let's say 100 ticks in LoRa mode, I don't get an RX timeout IRQ at the end of the timeout.I have checked the radio status with SUBGRF_GetStatus(). The radio goes to RX then back to standby.I have cross-chec...