User Activity

We have encountered issue with WB55 BLE firmware where it doesn't accept AD_TYPE_COMPLETE_LOCAL_NAME longer than 9 characters We have reproduced that issue on p2pServer example where we've modified local_name to be "123456789" all is OK.static const ...
We were experiencing strange crashes originating from HAL_SPI_TransmitReceive and HAL_SPI_Receive when operating in SPI Slave mode.Issue is that STM32 HAL code is not handling cases for 8 bit SPI Transfers correctly causing overflow of user buffers a...
We have project for STM32F405 configured and code generated with STM32Cube 5.x.x.x.After installing Version 6.0.0.0 and when project was migrated to STM32Cube Version 6.0.0.0 and code regenerated, all IRQ priorities for peripherals (UART, SPIs, I2C, ...
We have encountered the following issue:STM32H753 Rev V embedded UART bootloader does not work as in rev Y and earlier.We've deployed quite a few rev Y devices and now when we got Rev V delivered on PCB boards are failing DFU GO command.This seems li...
We have deployed quite a few of our products using STM32H753(ZIT6) rev Y and all was OK. All recent ones that we have around are rev V and they have issues with DFU bootloader over the UART. None of the issues that we have are listed in ERRATA notes ...
Kudos from