cancel
Showing results for 
Search instead for 
Did you mean: 

P-NUCLEO-LRWAN2 Debug Problem

KKoc.1
Associate

Hello, I bought this development kit to learn LoRaWan technology and improve myself.

P-NUCLEO-LRWAN2

STM32 Nucleo pack LoRa™ HF band sensor and gateway.

I made the connections of the product as written in the User's Manuals and saw that the product was working. I received the sensor data in the LorIOT portal without any problems. In other words, both the Gateway and the sensor board are working without any problems.

Then I wanted to make changes on Code and I downloaded I-CUBE-LRWAN software expansion for STM32Cube (UM2073) from ST.Com and opened it in STM32 Cube IDE. I compiled the code without any problems and uploaded it to my I-NUCLEO-LRWAN1 board without any problems.

When I start the debug process, it gives this error.

"Target is not responding, retrying..."

"Error! Failed to read target status

Debugger connection lost.

Shutting down..."

I also get this error message when I stop the Debug process after this error.

 0693W00000GYyCTQA1.png 

Where am I going wrong?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Andrew Neil
Super User

Sounds like the Target is going to sleep, so the debug connection is lost.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.