STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Bluetooth Mesh Library Capabilities

The Bluetooth Mesh Library version 1.14.0 has the following Capabilities:[Library Capabilities]Net Keys = 3App Keys = 3Elements per Node = 5Models per Element = 11Subscription per Model = 10Is it possible to increase these value somehow? I want for e...

CBuch.1 by Associate III
  • 3073 Views
  • 4 replies
  • 3 kudos

Resolved! Can't program/connect STM32WL55CC unless Hot Plug, why?

Hi, I have new custom board on STM32WL55CCU7. I can't flash/program with STM32CubeIDE. And when i try to connect with STM32CubeProgrammer with "Normal'" mode I have this error :"Error: Cannot connect to access port 1! If you are trying to connect to ...

LEdou.1 by Associate III
  • 5749 Views
  • 4 replies
  • 0 kudos

Need Help on transmitting audio over BLE - STM32WB5MM.

Hi,I'm Using stm32wb5mm-dk with I2S mic to capture audio and using TAS2563 I'm playing the captured audio. The data from the mic is transmitted and played using DMA. Now I want to transmit the I2S mic data using BLE. I used notification method using ...

LR.2 by Associate III
  • 2054 Views
  • 5 replies
  • 0 kudos

[BLE] Updating the stack

Would like to update the ble stack of stm32wb55 to 1.15.Do old commands from stack 1.13 are supported?And which parameter describes the stack version:APP_DBG_MSG("Wireless Firmware version %d.%d.%d\n", WirelessInfo.VersionMajor, WirelessInfo.VersionM...

DS.4 by Senior II
  • 924 Views
  • 1 replies
  • 1 kudos

Resolved! STM32 Programmer cli not working for MCU?

I connected my STM32WB5M DK with USB DFU mode according to manual and description.When i want to read or write the opt area over the cli and i got the error:Error: OTP programming is currently not supported on MCU devices What does it mean it is curr...

0693W00000Y94ReQAJ.png
CBuch.1 by Associate III
  • 1796 Views
  • 2 replies
  • 0 kudos