NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,Is it possible to work with one STM32WB central role as router in BLE and in LLD mode?As router I mean communicate in BLE to one smartphone and communicate in LLD with several remotes.The issue is that the CM0 coprocessor firmware is different ...
We have a design implementing the STM32WL55/WE5.The recommended crystals on the reference designs and literature are:NX2012SA 32.768KHz EXS00A-MU00527X2NX2016SA 32MHz EXS00A-CS06465I want to verify that it is OK to use the following:For NX2016SA: EI...
Hello,I am trying to design a BLE custom template application. I start by following the STM32WB Bluetooth® LE - STM32CubeMX Application Conception (https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_BLE_STM32CubeMX) using the P-NUCLEO-WB55 board ...
My biggest issue currently is on my external app which is connecting to the WB that it cannot get the descriptor.As I debug using BLE using LightBlue there is no descriptor in my characteristic. As I notice recently by reading again the manual there ...
is there any STM32 variant which has on chip IoT/ WiFi connectivity module. So that it can be configured and used just like USART or timers.Regards
Hello,I'm using the exemple for FUOTA in STM32WL for single core (STM32WLE). And I would like to know where I can find the .ioc file to change the pinout confirguration of the chip.Thanks
Hello, I am trying to configure a custom board with STM32WB5MMG in STOP2 low power mode. For that, the program calls the PWR_ExitStopMode() function when a timer reaches 10 seconds and exits when EXTI0 interrupts by calling PWR_ExitStopMode(). Th...
Hi,I'm trying to set a custom board with STM32WB5MMG into low power mode STOP2. For that, program calls PWR_ExitStopMode() function when a timer reaches 10 seconds and exits when EXTI0 interrupts by calling PWR_ExitStopMode().The MCU goes into and ex...
As the title suggest I only receive data once. I also tried using HAL_UART_Receive_DMA and HAL_UART_Receive_IT still got the same result (only receiving once). I'm using Teseo-LIV3FL GNSS module and I've tested it before on my ESP32 and it works as e...
Hello!I use two stm32wl55jc1 boards for a point-to-point connection via LoRa, simple, without a gateway. Everything goes well until I introduced the possibility to change the communication parameters (press a button and enter on UART). After the inpu...