NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello ST-Community,I have two NUCLEO64 STM32WL55JC1 development boards and am trying to get the LocalNetwork example up and running. A build can be easily generated from the LocalNetwork_Concentrator in the CubeIDE and transferred to the board. On th...
Hi Guys,I have problems reading. I have followed the STM32WB Workshop on stm32wb (using mx version 5.4.0). Now i'm trying to read but all examples seem to only use notifying and writing.I have the following char created and added some default value.a...
Hi, am working on a STM32WL55 solution that has both Hi power (RFO_HP) and Low power (RFO_LP) circuitry included (like that of the WL55 Nucleo PCB, either one of which is used at a time). Am at a component placement situation where the VR_PA signal l...
Hi, I'm using the CM4 core to receive the data and store it in the SD card, once the FATFS only works on this core. Furthermore, I want to send this data via LoRa, but it only works on the other core (CM0Plus). How can I share this information betwee...
Hi,I have a project where im using the STM32WB5MM-DK to develop code to act as a ble P2P client. I have the development board setup as a P2P client and the code is working fine. but when introducing the code to initialize the onboard OLED screen my B...
I would like to implement UHF transmission with QPSK modulation using the STM32WL. The required data rate is slow, so direct control of modulation may be possible if the transceiver peripheral cannot achieve it natively. Has anyone managed this, or t...
Hello,Can anyone help me on how to receive characters from STM32WB55 to the USB DONGLE as a receiver to show the ADC values. Or send the values via BLE Gatt to an android application using the inbuilt BLE services in STM32WB55.The material offered a...
We are using STM32WB55RE in our application. we are trying to achieve ~10uA current consumption in sleep. But, 22uA(stable for 10min) immediately after entering sleep. After 10min current consumption start decreasing eventually to 14uA in next 60min....
I have used UART example code for P-NUCLEO_WB55 board to check it's UART.Now i want to share that project to another team memberBut if i just Copy paste project folder to other file location than it gives me compilation errors of Few files missing.I ...