STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WL55 PWM doesn't have deadtime option

Hi,I'm working on STM32WL55JC board and run "TIM_PWMOutput" example that run 4 PWM channels with diffrence pulse width.I'm trying to add deadtime between the channels (following this hands-on video https://www.youtube.com/watch?v=rDaC2N-33Oo  Minute ...

STM32WB55 external clocks(32.768KHz, 38MHz) not working

Hello AllI have a cutom board. I am working on STM32WB55VGQ6(BGA129).2 crystals(32.768KHz, 38MHz) output waves are not coming.I checked waveform by using an oscilloscope and OSC-IN/OUT pins are ground level(0V)Voltage conditions all 3.3V : VDD, VDDUS...

BLE not advertising - STM32WB5MMGH

Hi,I'm working with stm32wb5mmgh to transmit data. The thing is BLE starts to advertise only in the debug mode if I upload it in the device its not showing. So what I did I turned on led when it starts to advertise as I mentioned in the below code.  ...

LR.2 by Associate III
  • 2706 Views
  • 3 replies
  • 0 kudos

STM32WBA52CGU6 circuit Diagram

Hi Team, I am searching for STM32WBA52CGU6 circuit diagram unfortunately not able to found out because the file was not found in our ST website. Kindly help me to get the exact circuit for my project purpose.

Sakthi by Associate
  • 2362 Views
  • 2 replies
  • 0 kudos

Sub-GHz and ADC DMA integration errors

Hi All,I'm using STM32WL55JC board which include Sub-GHz, ADC and DMA peripherals (and many more of course)I run "ping pong" example to create Sub-GHz communication sucssfully, also run "ADC_SingleConversion_TriggerTimer_DMA" and changed to circular ...

Example of low power consumption for B-L072Z-LRWAN1

Hello,I use B-L072Z-LRWAN1 and I would like to know how to use it in very low power consumption. By default on mbed OS 6 with one hand with only one ThisThread::sleep_for(3s) I have a consumption of 10.45mA. I take my measurements with an amperemeter...

DuCanard by Associate II
  • 2676 Views
  • 4 replies
  • 1 kudos