STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Can not connect STM32WB55CGU6 with ST link

I'm using STM32WB55CGU6 (UFQFPN-48) for a design and trying to connect with the ST link. But seems like it is not connecting in any way.  Can anyone tell me how can I connect this MCU and upload the firmware to this MCU? Why it is not responding?  

MKDas_0-1689064113929.jpeg MKDas_1-1689064122169.jpeg
MKDas by Associate II
  • 7041 Views
  • 15 replies
  • 0 kudos

STM32WLE5JCI6 all bands activation

We are probably need a support from the ST team with the implementation of the LORA (STM32WLE5JCI6) supporting all four frequency ranges.ST has provided two reference designs, one for LB, one for HB. We have combined them together and made it not on ...

EGola.1 by Associate II
  • 1382 Views
  • 0 replies
  • 0 kudos

Resolved! Spurious BLE disconnection

Hi,I am using two device that are connected one to another with BLE.The first device is a server.The second is a routeur.I detect some spurious disconnection between both device after some random time.The disconnection error I get is : HCI_CONNECTION...

What is the maximum value of HS_STARTUP_TIME for BlueNRG-1?

Hi friend,I want to extend the HS_STARTUP_TIME for BlueNRG-1. What is the maximum value of HS_STARTUP_TIME for BlueNRG-1? I saw the datasheet AN4494 it says that "XTAL_startup = XTAL_startup_measured*1.2*1.1*1.3 = 1.716*XTAL_startup_measured".  So 19...

TWu.6 by Associate II
  • 804 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WB10CC RF output stage design question

Hello, For a personal project, I am designing a device that receives GPS data and transmits the UTC time information to other devices over BLE. I will also be designing a device that receives the data and displays it. For this, I have chosen the STM3...

77volatile77_0-1690045960408.png

STM32WB55 Trace Configuration Issue - No Trace Data

I've been working with the STM32WB55 microcontroller and have been trying to set up 4 bit trace functionality (ETM, not SWO) for debugging. I've connected the trace pins according to the datasheet and configured them in the STM32Cube software.Specifi...

TAtte.1 by Associate II
  • 2416 Views
  • 1 replies
  • 0 kudos

Cascading LPTIM in STM32WL55JC17

I'd like to know if it is possible to cascade two LPTIM in order to make a 32-bit counter. I'm implementing my main LoRa application with the sequencer but I need to have 32-bit hardware counter running continously in the background to count external...

JPablo1 by Associate II
  • 1709 Views
  • 1 replies
  • 0 kudos

Resolved! BLE Advertising Problem

Hello,I am working on a STM32WB55RG BLE Project and the problem is that about once in every 3 program that I upload, BLE doesn't work. After reupdating the BLE Stack firmware, it works correctly. I am using the BLE firmware v1.16.0.4.  What could be ...

Yusuf by Associate III
  • 2022 Views
  • 2 replies
  • 0 kudos