STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 226 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4068 Views
  • 0 replies
  • 3 kudos

Nucleo stm32wba65 current measuring

I want to measure current draw on a Nucleo-WBA65RI board using a Nordic PPK2 power profiler. I put the PPK2 in ammeter mode across JP2 of the Nucleo board, and loaded the BLE_Power_Central example in IDE. The Nucleo board is being powered by the USB ...

SLevi.1 by Senior
  • 254 Views
  • 0 replies
  • 0 kudos

How to config STM32WB55 BLE connect Window Size?

When I use an STM32WB55 as a Central to connect to another STM32WB55 acting as a Peripheral, I find via a sniffer that the Window Size in the connection parameters is 3 (3.75 ms). However, when I connect the same Peripheral with a mobile phone, the s...

lbo.1 by Associate II
  • 457 Views
  • 2 replies
  • 0 kudos

Resolved! BLE advertisement of ble_p2pServer on stm32wb05kz

I am trying to use the ble_p2pServer example on my stm32wb05kz, but it is not advertising and not detectable on the ST toolbox application. These are the debug statements I am getting via UART: *** UART Test - System Starting ***BLE Stack initialized...

NVM Option CubeMX

Could you add NVM option for zigbee stm32WB55 in cubeMX ?It's essential for developement of application (persistence and coord association...)thanks FYI: This is a repost from https://community.st.com/t5/stm32-mcus-wireless/stm32wba-option-nvm-not-pr...

Exeu by Associate III
  • 271 Views
  • 1 replies
  • 0 kudos

STM32WB55 no longer supported in X-Cube-Matter v1.5.0

Hi ST Team,I just downloaded X-Cube-Matter package v1.5.0 and noticed that support for STM32WB55 uC was entirely removed, without even being mentioned in the release notes. Why is that? Is the uC being discontinued?Where can I find updated Matter exa...

AViva.1 by Associate II
  • 320 Views
  • 2 replies
  • 0 kudos

STM32WB55 BLE stack is not giving RSSI

le_advertising_event = (hci_le_advertising_report_event_rp0 *) p_meta_evt->data;int8_t rssiValue = (int8_t) le_advertising_event->Advertising_Report[0].RSSI;We are using the BLE stack version full stack = v1.24.0.3 (we had older version 1.18.0.3 but ...

Resolved! STM32WL55 & FreeRTOS - Change system time base

Hello, I am working with the STM32WL55 core and I started the FreeRTOS test and a problem occurred to me that I would like to share with you.The only thing I have done is define pin 15 of port B as output and I have created a FreeRTOS task, and withi...

hluyo_0-1706060373735.png hluyo_1-1706060394133.png
hluyo by Associate
  • 3724 Views
  • 6 replies
  • 0 kudos