STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 226 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4068 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WL5MOC LSE 32kHz accuracy

Hi,  In the STM32WL5MOC datasheet I can find the 32MHz TXCO HSE accurancy, but not the LSE 32kHz RTC clock accuracy. Could someone look into this and provide the min/max values similar to TXCO characteristics in Table 10? Best Regards,Dave

50_ohm by Associate
  • 295 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WBA52 Standby Mode Example

Hello all,Anyone successfully implemented the Standby Mode for STM32WBA52/55?  I am struggling going thru the examples and I wouldn't be able to enter the standby mode level.  My board still consume about 70mA when I enter the standby mode.  From the...

Resolved! Can't Program or erase NUCLEO-WL55JC1

I have just received 2 NUCLEO-WL55JC1. Upon connecting either one of them via I see The Red (main power) and green LEDs on. The other thre are flashing alternatively (red, orange, blue). I haven't changed the default jumper settings.The following deb...

mapfumo by Associate
  • 453 Views
  • 2 replies
  • 2 kudos

DIMMABLE COLOR LIGHT callbacks never invoked

Hi there and happy new year! I am currently trying to develop a dimmable color light with an stm32wb55 (Nucleo Board). Everything seems to work when connecting the device to a zigbee2mqtt server over zigbee. But actually all color server related call...

Exeu_0-1767261198328.png
Exeu by Associate III
  • 391 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB55 freezing when returned from STOP2 after RTC wakeup

Hello,I modified the BLE Beacon example to send 5 beacon packets and then enter into the STOP2 mode. It is possible to wake-up and resend 5 packets when a button is activated. However, when the time is set, the MCU wakes-up, and freeze.The function U...

fo by Associate II
  • 780 Views
  • 2 replies
  • 1 kudos