cancel
Showing results for 
Search instead for 
Did you mean: 

Using an NFC Antenna with the STM32WBMMG

Hbburnha
Associate II

I am wanting to add the STM32WBMMG to my board but it will need to be compatible with an external NFC antenna so I can have cellular communication. 

Is this possible and how would I go about implementing this?

If it is not possible are there other STM modules that are NFC compliant? 

 

 

1 REPLY 1
STTwo-32
ST Employee

Hello @Hbburnha 

The NFC use the 13.56 MHz frequency. But the STM32WB does support the 2.4GHz frequency. So, it should not be able to work for NFC. For NFC proposition from ST, you can have at the NFC (Near-Field Communication) and RFID - STMicroelectronics.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.