User Activity

I'm trying to convert the BirdNET-Analyzer (https://github.com/kahst/BirdNET-Analyzer/tree/main) model to run on a STM32U5A5. However, both the TFLite and STM32Cube.AI MCU Runtime fail.The TFLite runtime fails with: Operator REDUCE_MIN not supported ...
I fear there is an error in the new Nucleo-U031R8 board. The D13 pin is labeled as the SPI1 SCK pin on the boards' silkscreen. However, the board schematic shows that this is connected to PA5. STM32CubeMX reports pin PA1 as the actual SPI1 SCK pin.So...
Kudos from