NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello, I'm trying to use STM32WLE5CCU6 MCU as a radio module transceiver.I have followed the MB1874_LowPower reference design down to it's 0.7 mm substrate thickness.I connected the internal MCU RF power supply pins required like in the reference des...
HI Madam Sir, Had anyone tried to port the cable replacement sample included in the Firmware package to STM32WB55CC? This MCU has different pins and FLASH sizes.Thank you.Ian C Mosquera
Hello!I'm currently trying to get two B-U585I-IOT02A (STM32U585AI) boards to communicate with UART over BLE. I'm using the BLE_CableReplacement example project (STM32Cube_FW_WB_V1.13.3/Projects/P-NUCLEO-WB55.Nucleo/Applications/BLE/BLE_CableReplaceme...
I have an STM32WB design using I2C to get 6 bytes from a BMI0888 every 50ms (triggered by an external interrupt). The interrupt sets a flag in my main loop to go get the data. The devices first requires you to write the desired register, then read ...
Hello,I want to be able to perform OTA updates of nodes in a bluetooth mesh network. Therefore I want to add a service and a characteristic to the existing BLE connection between a proxy node and a smartphone/PC. Currently, only the mesh provisioning...
Curious regarding using ACI_GAP_SET_AUTHENTICATION_REQUIREMENT to change the fixed pin after already using a different pin key for a previous connection. Would that work? Any bad consequences?
Hi can MCU STM32WL33 - QFN32 work with the balun BALF-SPI-01D3? Where can I find the solution on 2-layer PCB (for 868MHz)? // for Antenna johanson 0868AT43.. regards zbyno
Hello community, I am trying to read a characteristic before each advertisement on BlueNRG-2 devboard. I started from the example BLE_Sensor_Demo, I adapted the services and characteristics. I want to use a characteristic as a flag. When characteri...
I created a custom application using the code from the BLE_THREAD_DYN example and the v10.0 FW BLE_THREAD_DYN stack. The BLE works fine but the thread stack goes down after a few minutes. The main differences between my code and the example is that I...
From the STM32CubeWB firmware package, there is a Thread_RCP project. However, there doesn't seem to be any documentation for it (it is not even mentioned in AN5289). The only hint is the readme.txt file which says: "This application is used to demon...