2023-05-28 1:13 AM
STLINK-V3PWR Not able to connect to STM32WL and other STM32 MCU's using STM32CubeProgrammer
Same MCU is working with STlink-V3
13:39:13 : ST-LINK SN : 002F004D3431510137383732
13:39:13 : ST-LINK FW : V4J2B1P4
13:39:13 : Board : STLINK-V3PWR
13:39:13 : Voltage : 0.02V
13:39:13 : Error: No STM32 target found
2023-05-28 11:35 AM
Apparently the measured Target MCU voltage is 0.02V, maybe there are some jumpers of switch to adjust to get setup working well.
2023-05-29 4:13 AM
Hi
I able to connect now using CubeProgrammer, After connecting TVCC to Target MCU VCC.
Without connecting TVCC to MCU VCC , STlink-V3 is working but not with V3PWR.
again V3PWR is still not working with CubeMX IDE.
Thanks
KarthiG