how can we generate a continuous waveform to measure the output power on a custom board using STM32WLE5CCU6.
Hi,
We are designing ou custom Lora application based on the STM32WLE5CCU6 MCU.
1- We would like to know if there is an eval board that can be used in manufacturing tests to perform a pingpong communication test (between our custom board and the eval board). Is there an AN that decribes such test ?
What we ve found is this document that can be used to perform a ping pong test.
Are there any other related documents ?
For the eval board we ve found two boards:
- https://www.st.com/en/evaluation-tools/nucleo-wl55jc.html
- https://www.st.com/en/evaluation-tools/stdes-wl5u2sbb.html
The later one do not have any mention to the STM32WLE5CCU6 MCU (Only STM32WL5)
Which eval board should be used ?
2- Is it possible to generate a continuous waveform from the STM32WLE5CCU6 MCU in order to make frequency and power measurements ?
Thanks
BR