STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! BLE not starting on original STM32WB55

Hello,Recently, I’ve been asking several questions about STM32WB55 BLE behavior, and the respected @FilipKremen  has provided me with great support.It turns out that all this time I was actually working with fake Chinese chips. I suspect that some of...

IlliaGx by Senior
  • 1050 Views
  • 6 replies
  • 6 kudos

Blue NRG-2 Bringup

On a custom board, I would like to use the BlueNRG GUI (v.4.7.1) to run the tests described in AN4818 (rev.8) using the DTM firmware embedded in BlueNRG-1_2 DK 3.2.3.I got a connection and I am able to send basic commands, like ACI_TEST_TONE START an...

Resolved! RM0473 Typo

Hello ST Community team,About the Typo, on the Table 1 of the RM0473, we have a reserved region between SRAM1 and SRAM2a (from 0x2000 3000 and 0x2002 FFFF) the size of this region is 180 Kbytes and not 36 KBytes as mentioned on the Doc.please have a ...

Issamos by Lead III
  • 245 Views
  • 1 replies
  • 1 kudos

Resolved! Confusion about PA impedance specification of STM32WL31xx

Hi!If I look at the datasheet of STM32WL31xx, I find Table 34. PA impedance which tells e.g. an optimum load impedance of 32 Ω // 16 nH in line 5 (high power, 868MHz) This STM32WL31xx is (according to the datasheet) available in VFQFPN32 and VFQFPN48...

Franz1_0-1767033671854.png
Franz.1 by Associate III
  • 569 Views
  • 3 replies
  • 1 kudos

LoRaWAN End Node DualCore on Linux

Hello, I'm having troubles building the two projects of the STM32 Nucleo WL55JC1 belonging to the LoRaWAN End Node DualCore Example under Linux (Ubuntu 24.04). It works on Windows 11, though.Until now I have all projects developed on Linux, this is m...

bgoedel by Associate II
  • 331 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WL5MOC LSE 32kHz accuracy

Hi,  In the STM32WL5MOC datasheet I can find the 32MHz TXCO HSE accurancy, but not the LSE 32kHz RTC clock accuracy. Could someone look into this and provide the min/max values similar to TXCO characteristics in Table 10? Best Regards,Dave

50_ohm by Associate
  • 287 Views
  • 1 replies
  • 0 kudos