STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! BLE disconnection problem on Android 15

I enabled the bonding feature in STM32WB5MMGH6TR.Bonding is working correctly. But when the device(STM32WB) is bonded to phone(Android 15), calling disconnect from the phone does not disconnect the device.This problem does not occur when:-1. Phone An...

abhi4_0-1766479530563.png abhi4_1-1766479549092.png
abhi4 by Associate II
  • 260 Views
  • 1 replies
  • 0 kudos

FUS,BLE update

FUS and BLE update.I would like to know if it is possible to update FUS (1.2.0)(2.1.0) and BLE (1.23.0) via SWD. I need to update two boards simultaneously and am having problems with programming via DFU. One of the boards always shows an error. I us...

STM32WL5MOC dual output bands.

This https://blog.st.com/stm32wl5x-stm32wl5m/ seems to suggest that the wireless module could be either 900 or 800 MHz bands."Hence, coupled with the wide frequency range supported by its STM32WL5x, the module can work in Europe, Americas, and Asia."...

NUCLEO-WL55JC1 Sleep Mode Current Consumption

  Hi, I am using the NUCLEO-WL55JC1 board and referring to the PWR_STOP2_RTC example to measure current consumption. I have isolated the ST-LINK section and am powering the board with an external 3.6 V supply for accurate measurement. However, in sle...

Screenshot 2026-01-08 162641.png
Deep23 by Associate II
  • 597 Views
  • 5 replies
  • 1 kudos

Resolved! DWT timing question

P-NUCLEO-WB55Just a sanity check really.I'm using the DWT unit to time a chunk of code, am I right that each tick is at 1/32MHz?

How to change advertisment data on BLE beacon

Hello. I got my hands on a wba55cg nucleo board and i'm currently studying about ble.I want to create a BLE Beacon that changes its adv_data whenever a user presses one of the button. From messing around using the p2p_server and beacon st examples, i...

AlexES by Associate III
  • 208 Views
  • 0 replies
  • 0 kudos

Ultra low power consumption using LPTIM

I am using LPTIM for pulse counting in ultra low power (stop 2) mode for STM32wl55jc. Now, the problem is on the pin if I connect any pull up/ pull down with 10k-50k range, it draws significant amount of current. Can anyone please suggest a circuit t...

Dhruv by Associate
  • 160 Views
  • 0 replies
  • 0 kudos