NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Dear ST members,My application is using the EEPROM emulated library (X-CUBE-EEPROM) with an STM32WB microcontroller. I noticed that, when I update a variable, the page can be padded with random zeros. Attached are screenshots of the page before and a...
According to BLE spec, whitelisting is not related to paired or bonded devices. Our application uses the advertisement and scanning for sensor beaconing application. STM32WB55 is not able to scan the interested sensors by whitelisting. STM32WB is not...
I just flashed the end node of the P nucleo LRWAN 3 with the AT master firmware, but I am still unable to send AT commands via my terminal to reconfigure some parameters of the end node. I also made sure I set up all the necessary parameters in the t...
Hello, Board: NUCLEO-WL55JC2 (2 boards)MCU: STM32WL55JCIDE: STM32CubeIDEProgramming: Bare-metal C or Cube IDE(C/C++) Goal:I want a minimal RF example using two NUCLEO-WL55JC2 boards where one board transmits a simple message and the other receives it...
Hi, I'm using a STM32WL5MOC. I see that in the LoRaWAN_Init the LmHandlerJoin is not in a USER CODE section, meaning that it can't be disabled. In my application I would like to do the join upon my request and not in the init. How I can prevent from...
Hello There i am using https://github.com/STMicroelectronics/STM32CubeWL/tree/main/Projects/NUCLEO-WL55JC/Applications/LoRaWAN/LoRaWAN_End_Node_FreeRTOS this example ,in that there is timer used for sent the data , i want RTC for send data for partic...
I am using STM32WBA5MMGH6TR in my project for sending data received from a sensor. BT is used for transmission.The data will be transmitted to a central node.This is a battery operated device. The signal chain is given below.Sensor--> ADC-->STM32WBA5...
Hi, I'm working with LoRa on STM32WL5MOC for a custom board and comparing performance with the dev board. I've measured RSSI and SNR at different distances. - Custom board vs Dev board RSSI, SNR values are noted for reference. How do I improve the ...
Split from STM32WBA5MMGH6TR Debug interface PCB layout - which is a separate question.Hi , thank you very much.In my module (STM32WBA5MMGH6TRTR), there is only one pin for boot selection BOOT0. I believe when it is pulled low booting happens from mai...
I am using STM32WBA5MMG in my design. This the development board schematic. Below image is from development board schematic.As per the constrains , SWDIO and SWCLK must be length matched. Also need to provide a shield.My questions are given below.SWD...