cancel
Showing results for 
Search instead for 
Did you mean: 

FreeRTOS on STM32: usage of MQTT and AWS

onvol2024
Associate

Greetings,

I am a beginner in STM32WB55 development and I have a project that requires using the SARA-R422M8S-00B module to connect to the AWS IoT core. I have installed FreeRTOS in the STM32Cube MX, but I am not sure how to use the core MQTT and AWS IoT libraries that are included in FreeRTOS. I have also faced many errors while compiling FreeRTOS. I would appreciate any guidance or resources on how to start this project. Thank you for your time and attention.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
STTwo-32
ST Employee

Hello @onvol2024 and welcome to the ST Community :smiling_face_with_smiling_eyes:

For your use case, I suggest you ask the same request on the FreeRTOS community. You may find more Resorces since your use case is related to the FreeRTOS features.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

mƎALLEm
ST Employee

Hello,

Refer to X-CUBE-AWS . It could help you and gives you an idea how to implement it.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.