STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 216 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4061 Views
  • 0 replies
  • 3 kudos

Resolved! Expansion Board with Quad SPI NOR FLASH

Are there any expansion boards with Quad SPI NOR Flash chips? I am interested in using it with a NUCLEO-WB55RG board.Preferably it should use the Macronix 25L6433FM2I-08G chip, but that is not a hard requirement. This chip is found on the X-NUCLEO-GF...

DavePfz by Associate III
  • 231 Views
  • 2 replies
  • 0 kudos

Resolved! How to design STM32WL55 with IPD for 865MHz

Is there any way to optimize the IPD BALFHB-WL-01D3 to work at 865MHz at 22dbm for STM32WL55? And is there any hardware design guide for power of STM32WL like it is there Hardware design guide for STM32L0 application note AN4467.

Resolved! ID and PAC query for Sigfox

Hello everyone, this is my first time using an ST microcontroller. Specifically, I am using the MB1389E (NUCLEO-WL55JC1) development board. It has been a bit confusing because most of the tutorials have an old version of STM32CubeIDE where everything...

Fer by Associate
  • 258 Views
  • 2 replies
  • 0 kudos

Resolved! Cannot Flash STM32WB55CEU6

Hello, I have a custom board with a STM32WB55CEU6 and I am trying to programm it through a Nucleo STLink with SWD. The onboard Nucleo CPU is detected and works fine if I add the jumpers, and I can program a different STM32 board with the jumpers remo...

Resolved! STM32WBA5MMG GND pads near antenna

Dear all, I have a custom PCB with the STM32WBA5MMG module. I missed the keepout requirement in the reference design and pads 2 - 5 and pads 56 / 59. These pads are connected to GND in my design. I did some signal tests, and I have a feeling the ante...

image.png

Resolved! STM32WL3x reference design - downloading program

Starting my design on a reference design based on STDES for WL3 series. I would like to know what is needed for the smallest hardware connection to download a program from ST32CUBE IDE. I need to have the minimum amount of connectors on the board. I....

KB1DC by Associate
  • 266 Views
  • 2 replies
  • 0 kudos