2024-07-19 7:39 AM - edited 2024-07-19 8:20 AM
When running second core initialization, the program goes into HardFault on line "i_feature = *(i + p_MBMUX_Cm0plusFeatureList->Feat_Info_TableAddress);"
The code was automatically generated by CubeIDE when opening the ST program "SubGHz_Phy_PingPong_DualCore"
---------------------------------------------------------------------------------------------------------------------------------------------------------
mbmux.c
static uint8_t MBMUX_CheckIfFeatureSupportedByCm0plus(FEAT_INFO_IdTypeDef e_featID)
{
int8_t ret = 0;
uint8_t i;
uint8_t cm0plus_nr_of_supported_features;
FEAT_INFO_Param_t i_feature;
/* USER CODE BEGIN MBMUX_CheckIfFeatureSupportedByCm0plus_1 */
/* USER CODE END MBMUX_CheckIfFeatureSupportedByCm0plus_1 */
if (p_MBMUX_Cm0plusFeatureList != NULL)
{
cm0plus_nr_of_supported_features = p_MBMUX_Cm0plusFeatureList->Feat_Info_Cnt;
for (i = 0; i < cm0plus_nr_of_supported_features; i++)
{
i_feature = *(i + p_MBMUX_Cm0plusFeatureList->Feat_Info_TableAddress);
if (i_feature.Feat_Info_Feature_Id == e_featID)
{
ret = 1;
break;
}
}
}
/* USER CODE BEGIN MBMUX_CheckIfFeatureSupportedByCm0plus_Last */
/* USER CODE END MBMUX_CheckIfFeatureSupportedByCm0plus_Last */
return ret;
}
--------------------------------------------------------------------------------------
features_info.h
typedef struct
{
uint32_t Feat_Info_Cnt;
FEAT_INFO_Param_t *Feat_Info_TableAddress;
} FEAT_INFO_List_t;
--------------------------------------------------------------------------------------
typedef struct
{
FEAT_INFO_IdTypeDef Feat_Info_Feature_Id;
uint32_t Feat_Info_Feature_Version;
uint32_t Feat_Info_Config_Size;
void *Feat_Info_Config_Ptr;
} FEAT_INFO_Param_t;
--------------------------------------------------------------------------------------
The structure has values but still crashes when i read from it.
Thank you for your help.
2024-08-13 8:30 AM
Hello @AlexandreMagno
Could you please give more details (are you using your own design or the B-WL5M-SUBG1, have you followed the run/debug steps mentioned on the readme file of the Project) I'm not able to reproduce this on my B-WL5M-SUBG1.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.