STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

Resolved! ADC with BLE onSTM32WBA

Hi,I want to implement a simple application: ADC conversion and transmit the data via BLE. I achieved to do it on stm32wb15cc development board, but I have problems when trying do implement it on my custom board with stm32wba54. In the codes, I basic...

Tony_Tony by Associate II
  • 2618 Views
  • 6 replies
  • 4 kudos

HeartRate FreeRTOS Default task

Hi all,I'm referring to BLE_HeartRateFreeRTOS example project. As per my understanding, controller wakes up to advertise based on the Adv Interval. This can be fast(80ms-100ms) or low power advertising(1s-2.5s).In this project there is a default task...

ABN by Associate III
  • 2705 Views
  • 5 replies
  • 2 kudos

Resolved! Beaconing advertisement

Hi all,I'm referring to the BLE_Beacon example project. I figured out that we need to start the advertisement and then attach the required payload/service_data. Is there any minimum set of advertisement packets to be broadcasted in-order to see the p...

ABN by Associate III
  • 1047 Views
  • 1 replies
  • 0 kudos

Resolved! Add Scan_Request to BLE_Custom example

Sono partito dall'esempio BLE personalizzato per il core WB55RG, che esegue regolarmente Advertising. Tuttavia, ora vorrei aggiungere una scan_request (sto cercando di replicare l'esempio P2P_router partendo da un esempio BLE_custom per avere servizi...

LoRaWAN FUOTA class C

Hey everybody,I am currently working on a project which involves a firmware update over the air (using the nucleo wl55jc1 board). i have found an example project through the official website (https://www.st.com/en/embedded-software/stm32cubewl.html) ...

Schermafbeelding 2024-12-04 151038.png IdiotStudent_0-1733927114845.png

Bluetooth Low Energy does notadvertising

Hi, I tried to setup BLE, I do not know how I managed first time to success - but I can't do it anymore :DOnce it was working and even tried to send characters, but now I cant setup it anymore.I follow up https://wiki.stmicroelectronics.cn/stm32mcu/w...

BLUETOOTH_0-1742577211047.png BLUETOOTH_1-1742577238015.png BLUETOOTH_2-1742577253064.png BLUETOOTH_3-1742577279388.png