STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32 LTDC TouchGFX GUI Glitching

What could be the cause of this glitch on my LCD-TFT screen? My system includes an F429 MCU, an SDRAM, and a 24-bit LCD panel. The interface was designed with TouchGFX, and the circuit board was designed by me.    

Trampler by Associate III
  • 3057 Views
  • 4 replies
  • 0 kudos

Changing default asset/ folder

Hi,By default, when you open a touchgfx project in the designer, images, texts and fonts come from the asset/ folder.How can I change that? I'd like to use another folder by default. I haven't found in the config files where this option is.Thanks in ...

GMeur by Senior II
  • 1684 Views
  • 7 replies
  • 1 kudos

Touchgfx with usb host CDC VCP

Hi everyone..I have issue here, I am using USB CDC VCP the applistate is not going into ready state, i tried alone with the usb host it is working correctly for this and also used example alsoTested configuration 1.Configured gpio pins for usb fs hos...

Resolved! Modal redraw question

Hi community!I'm using Touchgfx 4.24.1 with a STM32H753ZIT6, integrated to a 1024x600 (RGB565) display. We use double frame buffer in an external SDRAM (parallel) with DMA2D enabled. This is a OEM custom board design for us, so the hardware is alread...

uilter by Senior
  • 2492 Views
  • 3 replies
  • 0 kudos